How to create a drawing related to an alternate representation

2021-10-06T23:26:07Z

Summary


Details

When creating a drawing of an alternate representation (altrep), the drawing relation automatically gets associated to the UGMASTER. How can a drawing be created referencing an alternate representation?

Solution

  1. In NX, select 'File-->Open' to open the altrep.
  2. Select 'File-->New' and select a drawing template to create the new drawing.
    NOTE1: In the File New dialog, consider naming the drawing dataset to match the name of the altrep dataset, so they are visually matching.
    NOTE2:  Do not save the new drawing yet.
  3. Switch to the Modeling application.
  4. In the Assembly Navigator, highlight the UGMASTER component, 'MouseButton3-->Delete'.
  5. In the Menu, select 'Assemblies-->Components-->Add Component' to add the altrep as an assembly component.
  6. Switch back to the Drafting application.
  7. Select 'File-->Save' to save the drawing.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0
Function: FILE_NEW

Ref: 002-8000640

KB Article ID# PL8000640

Contents

SummaryDetails

Associated Components