Why Inspection path is not created in line feature direction (bi-directional) even if reverse direction is applied
Solution
The line created by the construction operation is a "derived object" (using the create new option) and should not be edited (this is true in general when using the create new option).
The sequence of features in the construction operation will set the direction of the constructed features.
The bi-directional associativity where changing the line direction causes the sequence of features to change in the construction operation.
Notes