Details
In ESI template, execute "Search Sleeve Position" of "Design ejector pin" command.
There is no response.
Can we use "Search Sleeve Position" option of "Design Ejector Pin" command in ESI template?
Solution
In function "Search Sleeve Position", It will search the part which has UM_SHRINKAGE properties and UM_PROD_BODY feature both. Then this part also need to have core region and cavity region. In this circumstances, it will search sleeve position.
In ESI template, the part with UM_SHRINKAGE properties does not have UM_PROD_BODY feature name. So there is no response.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: KDA
Version: V11.0.1
Function: MOLDWIZARD
Ref: 002-8000594