Routing components cannot be moved with "Anywhere in Assembly" scope

2021-10-06T23:26:06Z

Summary


Details

When "Anywhere in Assembly" move component scope is set in customer defaults, 
if the user attempts to move a routing component that is connected with a routing path by "Move component" command, the component returns to its original position and could not be moved

Solution

"Anywhere in Assembly" move component scope is not supported for moving a connected routing component.


The user needs to set "Work Part Only" move component scope in customer defaults for moving a connected routing component.


NX11 onwards an alert message is displayed as follows.


 Alert:


A selected component is in a Routing part and hence cannot be moved as the Move Component Scope is set to Anywhere in Assembly in Customer defaults.


 



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: NX
Application: ROUTING_GENERAL
Version: V10.0.3
Function: PART

Ref: 002-8000517

KB Article ID# PL8000517

Contents

SummaryDetails

Associated Components