Details
User getting a license error on the client system hosting solid edge licenses on the Windows Client OS
If we click on perform status enquiry it shows error of host ID.
Also it does not allows to run solid edge locally.
But Solid Edge can be run on client machines
Solution
Ping the hostnames of the same system and getting a General Failure message
The Solid Edge license manager was hosting the licenses successfully and these licenses were consumed on the client system pinging the hostname of the Solid Edge license manager
The system not pinging its own hostname could be a Firewall/Anti_Virus setting or an OS setting
The information on "General Failure" error message has been discussed in the below links:
-http://www.corenetworkz.com/2011/08/ping-transmit-failed-general-failure.html
-https://answers.microsoft.com/en-us/windows/forum/windows_7-networking/resolved-ping-transmit-failed-general-failure/53b05029-1da8-4f68-8eb4-221a343e97e1?page=2
-https://social.technet.microsoft.com/Forums/windows/en-US/923dc99b-0ec2-48af-8199-282568471aa6/ping-and-tracert-return-general-failure?forum=w7itpronetworking
-https://superuser.com/questions/433416/why-do-i-get-general-failure-when-pinging-host-name-on-a-win-7-node-on-the-net
-https://forums.techguy.org/threads/solved-general-failure-message-on-command-prompt-when-ping-a-ip-or-dns.695935/
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: SETUP
Version: V109.0
Function: LICENSING
Ref: 002-8000173