License error at Client system

2021-10-06T23:26:05Z

Summary


Details

Reconnection Failed
Cannot connect to the server (Error occurred: -15)
Do you still want to save changes?

Solution

-Access the License server machine .
-Check if the LAN card for which the Composite ID has been registered has been enabled.
-Check Firewall/Antivirus on the License Server and add the lmgrd.exe, lmtools.exe, ugslmd.exe and the license file port number into the exceptions of the Firewall
-Check whether the license server system can be "telnet" using the license file port number from the client system


 Once the license server and the client system communication is established, the client will get the licenses from the license server

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSTEM
Version: V11.0
Function: SYSTEM_TOOLS

Ref: 002-8000113

KB Article ID# PL8000113

Contents

SummaryDetails

Associated Components