NX Maintenance Release Update Error

2021-10-06T23:26:05Z
NX System Administration

Summary


Details

Getting an error while updating the Maintenance Release as below:


 Install failed
Error 255 from running
D:\NX_Patch02\dvdrom1102_nx\ugs_update1102\ugs_update.bat /p and 1

Solution

Check the account rights for the logged in user and he is the admin user
-Tried running the ugsupdate through the batch file, command prompt and the UI still getting the same error


 -NX has been installed with the folder name as NX11 (Do Not Delete)
-The existence of the bracket and the empty space in the installed folder not supporting the MR installation


-Uninstall of the present NX version and Reinstallation resolves the issue of patching NX to the latest Maintenance Release

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSTEM
Version: V11.0.2
Function: WNT_INSTALL

Ref: 002-8000109

KB Article ID# PL8000109

Contents

SummaryDetails

Associated Components

Installation Licensing Plotting