Siemens PLM Licensing License Error: cannot connect to license server system. The server ( lmgrd ) has not been started yet, or SPLM_LICENSE_SERVER is set to the wrong port @host [-15]

2021-10-06T23:26:05Z
Licensing Maintenance

Summary


Details

User unable to deploy a license file and getting the license error as below;
License Error: cannot connect to license server system. The server ( lmgrd ) has not been started yet, or SPLM_LICENSE_SERVER is set to the wrong port @host [-15]

Solution

Check the license file and verify if it is a Floating license or a Node Locked license


 This could also be a node Locked license 


In case of Node Locked license, specify the path of the license file including the file name in the system variables of a client system
This should resolve the issue

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSTEM
Function: SYSTEM_TOOLS

Ref: 002-8000107

KB Article ID# PL8000107

Contents

SummaryDetails

Associated Components

Siemens PLM Common Licensing