Details
-User has a Solid Edge Base Floating license (solid edge classic)
-User wants to add a Solid Edge add-on license (wire harness) of Node Locked type to the license file
Solution
A Solid Edge license cannot have the base license of Floating type and an add-on license of Node Locked type in the same license file
A mix type of authentication is not a possible option in case of Solid Edge. Either all the licenses (base and add-on) should be Floating or Node-Locked.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: SETUP
Function: LICENSING
Ref: 002-8000098