Simcenter 3D Solutions How to Display an Element X Axis Vector

2021-10-06T23:26:05Z
Simcenter 3D

Summary


Details

The user wishes to see a vector representation of the element X axis.

Solution

Assuming no material orientations have been defined, the elemental x axis of shell elements or any of the solid element axes can be displayed using the "Element Material Orientation" command in "Finite Element Model Checking".  Select the desired elements, select output  vector options, and select the "Display Element Material Orientation" box.   If material orientations has been set, it is necessary to be reset them 

in order to see element coordinate system orientations.

Notes

KB Article ID# PL8000080

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow