Information about update Hole Table in NX

2021-10-06T23:26:04Z

Summary


Details

How to update new Holes added to the model in the Hole Table.

Solution

As it mentioned in the NX Documentation "update a hole table" method.
This method is working if user select a View as an Object to create a Hole Table.
-----------
Right-click the Hole Table Section and choose Update Hole Table.
The new hole appears in the table and is labeled in the view.
--------------
If user creates Hole Table by selecting the holes one by one, this method can't work.
User should select Hole Table-MB3-Edit, and select new created Hole to add it to the Hole Table.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: DRAFTING
Version: V11.0
Function: DIMENSION

Ref: 002-8000052

KB Article ID# PL8000052

Contents

SummaryDetails

Associated Components