Solid Edge Frame Options Dialog clipped

2021-10-06T23:55:29Z

Summary


Details

--------------- 
When using "Frame Options - Expand", the form height of the Options Dialog 
is too small -- the complete information cannot be seen.



Solution



When a user invokes the Frame Options the first time and makes some 
modifications Solid Edge will create some registry keys in 
HKEY_Current_User including the form height of the Frame Options dialog. 


The stored height is too small when the registry keys were created when the 
Frame Options is collapsed.


This happens for example when you just move the collapsed Frame Options 
Dialog to a different position on the screen.


Modify the following registry entry manually:


1. regedit 
2. Navigate to 
 [HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\ 
 Version 109\General\Position\FrameOptions] 
3. Change the value of the dword "Height" to "772" decimal 
 which is "304" hexadecimal



Notes and References

Problem Report 8946615
This problem have been fixed with Solid Edge Version 2020.



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V109MP8
Function: FEATURES

Ref: 002-7009867

KB Article ID# PL7009867

Contents

SummaryDetails

Associated Components