NX Last used directory is showing blank Folder Name in NX

2021-10-06T23:27:13Z
NX for Design

Summary


Details

--------------- 
Last used directory is showing blank Folder Name in NX 
Issue is with last used Directory Path showing Blank Information. User was 
saving the data in any other directory other than Newstuff folder but in 
next session it does not use the last used directory path and its shows the 
blank information in File New dialog.



Solution

 Follow below steps to fix this issue with NX File New dialog. 


Reset Dialog Memory from NX [File >> Preferences >> User Interface >> Options 
Tab >> press "Reset Dialog Memory" button]. This is one time activity, if you 
are moving from older NX version to NX11 or later.



Notes and References

8864519



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: NXMANAGER
Version: V11.0.1
Function: FILE_NEW

Ref: 002-7009827

KB Article ID# PL7009827

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX