Details
How do I share Solid Edge data with suppliers from Teamcenter?
Solution
Use the SEEC Create Package command to create an unmanaged Solid Edge data set.
You can open the SEEC cache assistant to see if the Create Package option is enabled.
If it is not enabled, you can enable Create Package in Teamcenter options by setting the preference "SEEC_Enable_CreatePackage =1" and then restart the Solid Edge session.
Notes and References
IR 8537676
Hardware/Software Configuration
Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC
Ref: 002-7009728