Adjusting the thickness display of model edges

2021-10-06T23:26:40Z

Summary


Details

--------------- 
How to adjust the thickness display of model edges in the Modeling application.



Solution

1.  In the Menu, select 'Edit-->Object Display'. 

2.  Select the model or solid to be edited. 

3.  OK the Class Selection dialog. 

4.  On the 'General' tab, adjust the 'Width' to the desired thickness. 

5.  OK the Edit Object Display dialog.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V10.0
Function: DISPLAY

Ref: 002-7009717

KB Article ID# PL7009717

Contents

SummaryDetails

Associated Components