How to create a PMI Detail view in the Modeling application

2021-10-06T23:27:04Z

Summary


Details

How to create a PMI Detail view in the Modeling application.



Solution

 1.  In the Part Navigator, hover the cursor over 'Model Views', 
      'MouseButton3-->Add View'. 

2.  Name the view. 
     For example: Detail View A 

3. Graphically zoom in on the feature(s) to include in the Detail view. 

4.  In the Part Navigator, hover the cursor over 'Cameras', 
     'MouseButton3-->Create'. 

5.  Select OK on the Camera dialog. 

6.  Hover the cursor over the new Camera View. 
     'MouseButton3-->Capture View'. 

7.  Hover the cursor over the new Model View (Detail View A), 
     'MouseButton3-->Save'.


The Detail Model View can be rotated and zoomed in or out. However, the 
original zoomed-in state can be brought back by highlighting the Model View, 
'MouseButton3-->Reset Orientation'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: PMI
Version: V11.0
Function: MODEL_VIEWS

Ref: 002-7009716

KB Article ID# PL7009716

Contents

SummaryDetails

Associated Components