Simcenter 3D Solutions Customer Defaults for Model Display do not propagate to the FEM

2021-10-06T23:27:00Z
Simcenter 3D

Summary


Details

--------------- 

The customer toggles on Display in the customer defaults for Simulation-Model 

Display-Geometry Stitch Edges and Geometry Free Edges. 

After restarting NX 11 and creating a new Fem, Menu-Preferences-Model Display 

does not have those options toggled on.

Solution

 The Model Display defaults are saved to the part, such that if a Template FEM 

is used to create the part where these defaults are not set, the "global" 

customer defaults will not be honored, as you are not really creating a new FEM 

from scratch.

To get around this, use the Blank Template when creating the FEM, or create one 

that has the defaults set as you'd prefer.

Notes

KB Article ID# PL7009710

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow