How to export family members without "Part is part family member" icon

2021-10-06T23:26:52Z

Summary


Details

--------------- 
How to export family members without "Part is part family member" icon from TC 
to Native NX through Command Prompt without disturbing the existing customer 
default settings.


Current methods used: 
Phenomenon 1: 
If use “UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT=1” to export family members from TC 
to Native NX, the icon “Part is part family member” will be displayed in “Info” 
column. 
Phenomenon2: 
If not use “UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT=1” and do the settings as below 
to export family members from TC to Native NX, the icon “Part is part family 
member” will not be displayed in “Info” column. 
1.Toggle off “Include Part Family Member Template Part” and “Ignore Part Family 
Member – Include Template Part” in Customer Defaults. 
2.Add “-fam=strip_status” into Command Prompt.


But customer don't want to change the default customer default settings before 
exporting family members.



Solution

 Customer can export the modified DPV file(which will help to export the family 
members without "Part is part family member" icon) to disk and point to the 
same during clone operation to get the desired results. 
Variable to be set is UGII_LOCAL_USER_DEFAULTS=path to the relevant DPV file. 
You can achieve the results without disturbing the existing defaults at your 
end.



Notes and References

IR 8936358



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: CLONE

Ref: 002-7009709

KB Article ID# PL7009709

Contents

SummaryDetails

Associated Components