Details
---------------
How to export family members without "Part is part family member" icon from TC
to Native NX through Command Prompt without disturbing the existing customer
default settings.
Current methods used:
Phenomenon 1:
If use UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT=1 to export family members from TC
to Native NX, the icon Part is part family member will be displayed in Info
column.
Phenomenon2:
If not use UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT=1 and do the settings as below
to export family members from TC to Native NX, the icon Part is part family
member will not be displayed in Info column.
1.Toggle off Include Part Family Member Template Part and Ignore Part Family
Member Include Template Part in Customer Defaults.
2.Add -fam=strip_status into Command Prompt.
But customer don't want to change the default customer default settings before
exporting family members.
Solution
Customer can export the modified DPV file(which will help to export the family
members without "Part is part family member" icon) to disk and point to the
same during clone operation to get the desired results.
Variable to be set is UGII_LOCAL_USER_DEFAULTS=path to the relevant DPV file.
You can achieve the results without disturbing the existing defaults at your
end.
Notes and References
IR 8936358
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: CLONE
Ref: 002-7009709