Solid Edge
Shaded view is masking other geometry on the draft when printed
2021-10-06T23:58:15Z
Design
Summary
Details
When printing a Solid Edge draft file that contains a shaded view, the shaded view is blocking, hiding, or masking other geometry and details on the printed file when compared to the draft file.
Solution
This issue can occur if the view border of the shaded view is overlapping other geometry on the Solid Edge draft.
4. Create a new 'DWORD (32 bit) value "STRETCHMASKBLT_VERSION" and set it to 1 e.g.
5. Exit the registry.
Recreate the draft print out.
If the issue is still not resolved after setting this value, selecting a different value for the STRETCHMASKBLT_VERSION switch may have better results. This DWORD value can set to any of the following:
0 = No masking for shaded drawing views. Best for non-overlapping views
1 = Experimental tiling algorithm
4 = ST4 algorithm
5 = ST5 algorithm
6 = ST6 algorithm (Default behaviour)
20 = V20 algorithm No masking (equivalent to 0)
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: SOLID_EDGE Application: DRAFT Version: V221.0 Function: FILE