Installing Solid Edge there is the following error:
An error occurred during the installation of assembly component {XXXXXXXX- XXXX-XXXX-XXXX-XXXXXXXXXXXX} HRESULT: 0x800736FD.
Solution
This error originates in the Microsoft Windows installer files and is not specific to Solid Edge.
Possible causes of this error include:
- The file indicated in the error message has been deleted by another application.
- A CreateFile/ReadFile operation has been interrupted by a driver in the file system stack.
- The Microsoft .NET framework is out of date.
The below options may resolve this issue:
As a first step, try restarting the computer and then running the Solid Edge installer again.
- Consider disabling firewall or antivirus software that may be conflicting with the installation.
- Consider disabling UAC.
- Consider right-clicking - Run as Administrator.
- Ensure that your Microsoft .NET framework is up to date.
If the above suggestions do not resolve the issue then it may be necessary to rebuild the workstation and install a fresh operating system.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: INSTALL
Ref: 002-7009701