Editing part in place, surrounding geometry is not greyed out

2021-10-06T23:55:15Z

Summary


Details

When editing a part in place in the context of an assembly, the surrounding geometry in the assembly is not greyed or dimmed out making working on the part in place difficult.



Solution

There is a Solid Edge option to control the dimming of surrounding geometry in the assembly when editing a part in place.


1. Select Solid Edge Options -> View. 


2. Check or turn on "Dim surrounding components during in-place edit..."


3. Select "OK" to save the preference change.


The surrounding geometry will now be greyed out or dimmed when editing a part in place.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219.0
Function: SELECTION

Ref: 002-7009700

KB Article ID# PL7009700

Contents

SummaryDetails

Associated Components