Solid Edge templates are missing from the File New screen

2021-10-06T23:55:33Z

Summary


Details

When attempting to create new files from the Solid Edge New screen there are no template files listed to select from.



Solution

If there are no template files displayed in the Solid Edge New screen, resetting the Solid Edge new template files setting should resolve this issue.


To reset the template files displayed in the Solid Edge New screen:


1. Close Solid Edge.


2. Open Windows Explorer.


3. Browse to "%APPDATA%\Unigraphics Solutions\Solid Edge\Version 110".


4. Delete "NewFileDefaultList.xml".


5. Start Solid Edge.


The template files used in the New screen will be rebuilt and should now be displayed and selectable.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V219.0
Function: OTHER

Ref: 002-7009698

KB Article ID# PL7009698

Contents

SummaryDetails

Associated Components