There is a Numeric Keypad and Full Keyboard icon appearing while in any command; also the View radial popup always stays on. How to eliminate these popups?
Solution
Under Roles resource bar, expand the "Presentation" folder and click on "Role Default".
(It is likely using Role Touch Panel at the moment which brings up the Radial Spot popup and Input Numeric popup.)
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: SYSENG
Version: V11.0
Function: UI_TOOLS
Ref: 002-7009679