NX Import part into TC using the same item type as it was exported

2021-10-06T23:27:10Z
NX for Design

Summary


Details

How to import the part back into Teamcenter using the same item type as it was exported?



Solution

When importing parts back into Teamcenter, select the "Use Type from Part file" option; this will allow the item type to import based on the item type of the part file.


Note 1: The toggle "Use Type from Part file" check box must be toggled on before selecting parts from OS to import.


Note 2: This functionality is only supported for parts created in NX10 or later.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 864
Product: NX
Application: NXMANAGER
Version: V11.0
Function: CLONE_IMPORT

Ref: 002-7009678

KB Article ID# PL7009678

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX