---------------
To update after a Hole Table was generated, a new hole was added to the model.
Solution
As it mentioned in the NX Documentation "update a hole table" method.
This method is working if user select a View as an Object to create a Hole
Table.
-----------
Right-click the Hole Table Section and choose Update Hole Table.
The new hole appears in the table and is labeled in the view.
--------------
If create Hole Table by selecting one by one holes, this method cant work.
User should need to be select Hole Table-MB3-Edit, and select new created Hole
to add it to the Hole Table.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DIMENSION
Ref: 002-7009584