---------------
If I select more than 5000 nodes and create a graph in "Evaluate Nodal Function
Response" of Response Simulation, only 5000 graphs will be created.
Is there a function to change limitation?
Solution
You can only evaluate 5000 functions at a time.
The limit was set to keep a user was blindly evaluating responses over the
entire model, which could lead to a huge amount of functions.
This is hard coded in Response Simulation
Notes