Fence selection in Simulation environment does not work

2021-10-06T23:55:16Z

Summary


Details

Selection of elements in Framing Simulation does not work, while selection via 
Pathfinder works.



Solution

The problem in fence select is seen here because the perspective view is turned 
on. This is a desired behavior and can be seen for other commands such as 
'check interference'. If the perspective option is turned off then we can use 
fence select to select all the components. 

Workaround : Turn off the perspective option under view tab--->style group.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: SIMULATION
Function: STUDY

Ref: 002-7009570

KB Article ID# PL7009570

Contents

SummaryDetails

Associated Components