Details
The customer wants to create a space as a separator in Bend Data when doing a
'Save as flat'. After adding the " " in the options, the " " gets lost and is
not included in the resulting DXF.
Solution
Just put the string with the following space in single/double quotation marks,
e.g. "SEQUENCE: ". These entries are kept in "SESMF.INI", and will show the
needed result in DXF:
TC_BENDDATA
1000
SEQUENCE: 0
Note the space between ":" and "0".
Notes and References
IR#8312590
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: SAVE_AS_FLAT
Ref: 002-7009561