About the message displayed when run 'Advanced Studio' command.

2021-10-06T23:27:18Z

Summary


Details

--------------- 
1. Start NX on a Virtual Machine (VM) or on a system which does not have 
graphics card. 
2. Create a new part. Create a simple block. 
3. From the 'Render' tab execute 'Advanced Studio'. 
Below message appears: 
The graphics device does not support Advanced Studio display.



Solution

 The 'Advanced Studio' command requires high end rendering. The graphics card 
is used for this purpose. If the graphics card is not found on the system 
then this message appears. 
Install the certified graphics card on the system where you want to use this 
command to avoid this message.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0.1
Function: VISUALIZATION

Ref: 002-7009550

KB Article ID# PL7009550

Contents

SummaryDetails

Associated Components