NX "System Studio Material" is not displayed on the Resource bar.

2021-10-06T23:27:00Z
NX for Design

Summary


Details

--------------- 
"System Studio Material" is not displayed on the Resource bar unless perform 
"Studio Task" in NX11.



Solution

 For a new part, the "System Scenes" and "System Studio Materials" palettes 
are created the first time the user enters any of the High End Visualization 
Render modes (True Shading, Advanced Studio, Ray Traced Studio) or the Studio 
Task setup environment (which runs in Advanced Studio mode). This is working 
as designed and is done this way because the contents of these palettes are 
specifically relevant to High End Visualization.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0.1
Function: VISUALIZATION

Ref: 002-7009547

KB Article ID# PL7009547

Contents

SummaryDetails

Associated Components

Modeling