Why the commands cannot be shown in the Custom Group

2021-10-06T23:26:58Z

Summary


Details

--------------- 
Steps to reproduce: 
1. Create a new file using Model template. 
2. Menu -> Tools -> Customize. 
3. Commands (tab) -> New Item -> Drag the 'New Group' and drop it to Ribbon 
bar. 
4. Drag and drop some commands to this group. 
5. Click on the chevron/triangle on this group. 
Note that commands are not shown in the group.



Solution

 This is expected behavior. "New Group" is a custom user created group. 
Custom containers do not have the concept of turning on and off visibility of 
the command temporarily. This is because there is no baseline for which to 
return. Commands can only be added or removed.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0.1
Function: UI_TOOLS

Ref: 002-7009546

KB Article ID# PL7009546

Contents

SummaryDetails

Associated Components