NX Model shifts in position when switching from Shaded mode to wireframe mode

2021-10-06T23:27:07Z
NX System Administration

Summary


Details

Model shifts in position when switching from Shaded mode to Wireframe mode.



Solution

This unexpected behavior can be due to corruption of the saved display facets for that body. It can be resolved by:


"menu > View > Operation > Facet Settings...", In the Facet Regeneration section, make sure the Delete Saved Display Facets toggle is enabled, and then press the Regenerate Facets button. This will delete the saved display facets in the part that's opened in session; saving the part after this step will avoid having to apply the workaround again.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: SYSENG
Version: V11.0
Function: VIRTUAL_REALITY

Ref: 002-7009540

KB Article ID# PL7009540

Contents

SummaryDetails

Associated Components

Installation