NX Why line font of the View Break line become the "Dotted Dashed" line?

2021-10-06T23:27:09Z
NX for Design

Summary


Details

Why does the line font type of the "View Break" line become the "Dotted Dashed" 
line instead of Solid font type?



Solution

 The setting which controls this line font type of "View Break" or "section 
lines" or any lines or curves is (Preferences - Object - Line font). 
If the line font for any reason is changed to dotted dashed, so will be the 
view break line or any other lines/curves created. 
It also depends on the templates to create a new sheet all your template parts 
should be stored with appropriate line font types.


Note : There is no way to change the existing view break curve created, we need 
to recreate these views.



Notes and References

IR 8896300



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V8.5.3
Function: DRAWING/VIEW

Ref: 002-7009534

KB Article ID# PL7009534

Contents

SummaryDetails

Associated Components

Drafting