How do you show a Center of Mass symbol in draft?

2021-10-06T23:55:30Z

Summary


Details

How do you show a Center of Mass symbol in draft?



Solution

You can show the Center of Mass block (symbol) in a draft sheet using the following steps:


Right mouse click on the view and go to Properties > Display > Parts List Options > List All. Under the assembly in the Parts List tree will be a Center of Mass displayed. Select it, then check the Show box > Apply > Ok. Update the view and the Center of Mass will be displayed as a small dot in the view.


Use the 'Center of Mass and Coordinate System Block' to show a symbol in the draft.


Go to Solid Edge Options > Annotation > Select block for 'Center of Mass' > select 'Apply' > Select OK > Update drawing view.


Solid Edge provides the following default block, COM, to display when either the center of mass or the coordinate system is shown in a drawing view. It is included in the draft templates. You can create your own blocks with custom graphics.



Notes and References

8833003



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DRAFT
Function: PROPERTY_TEXT

Ref: 002-7009498

KB Article ID# PL7009498

Contents

SummaryDetails

Associated Components