Details
---------------
How do you set the Round-off precision preference of Angular dimensions?
Solution
You can set the Round-off precision preference of Angular dimensions from [Style] command.
Units tab (Dimension Style and Dimension Properties)
---------------------------------
Angular
Sets the units for an angular dimension.
Units-
Sets the dimensioning units for an angular dimension. This can differ from the working units of the document for the current dimension style in use. These settings are file specific.
Round-off:
Sets the round-off for the angular dimension value. This control is sensitive to the unit setting (decimal or fractional) and contains values as appropriate for the unit. This control is also sensitive to the dimension being placed and contains values as appropriate for the dimension.
--------------------------------
Angular tolerance-
Sets the units for angular tolerance. The options in this section apply when the Dimension Type is set to Tolerance (unit). They are not applicable when the Dimension Type is set to Tolerance (alpha).
Units
Sets the dimensioning units for angular tolerance. This can differ from the working units of the document.
Round-off
Sets the round-off for angular tolerance values.
Notes and References
7976890
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DRAFT
Version: V219.0
Function: ANNOTATIONS
Ref: 002-7009495