NX Arrangements are not imported to the last level of an assy structure

2021-10-06T23:26:57Z
NX for Design

Summary


Details

--------------- 
Arrangements are not imported to the last level of an assembly structure 
Customer has to perform Force save all after import to get the arrangement 
synced between NX and TC.



Solution

 Have the customer default "synchronize Assembly Arrangements" set to ON under 
File - Utilities - Customer Defaults - Teamcenter Integration for NX - General 
- Assembly section. 
Also toggle ON "Publish Optional Information" on the Import dialog under Other 
Parameters section. 
All the assembly structure would be in sync between NX and TC(All levels) with 
arrangement information during import assembly activity.



Notes and References

IR 8891550



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0.1
Function: CLONE_IMPORT

Ref: 002-7009482

KB Article ID# PL7009482

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX