Details
---------------
refile_err.log file is not getting created in NX11.0.1MP02 on executing
nxrefile.bat for NX translation, if translation is successful.
If there is any error in the translation, then it creates the refile_err.log
file
Solution
As per the new design change from NX11 onwards, creation of refile_err.log
file is only for the errors and is has been stopped creating the same for
successful refile operations.
Notes and References
IR 8889003
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0.1
Function: UTILITIES
Ref: 002-7009400