Details
---------------
Changing the drafting preference for the Balloon diameter does not change in
balloon dialog.
Solution
The Balloon symbol dialog uses dialog memory to store the last used symbol
size. Changing the symbol size in preferences will not affect the size
that is stored in the dialog, unless the dialog memory is refreshed. The
dialog memory can be refreshed by selecting the Reset button in the upper
right corner of the dialog.
Notes and References
Reference PR#6235611
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V12.0.2
Function: ANNOTATION
Ref: 002-7009331