NX Validation rule sets when importing assembly into teamcenter.

2021-10-06T23:26:58Z
NX for Design

Summary


Details

--------------- 
When using the Import Assembly into Teamcenter dialog, you have the option to 
run validation. When the "Validation Rule Set File Browse Option" is set to 
Teamcenter and selecting the Browse button, what type of dataset is it looking 
for?



Solution

 A Rule sets file can be stored in Native NX as *.vrx files, and in 
teamcenter as "ValidationRuleSet" datasets. When you select the Browse 
button with the "Validation Rule Set File Browse Option" set to Teamcenter, 
expand the Item that contains the dataset and select the Validation Rule Set 
dataset.


You can test by creating a new item in Teamcenter, then add the 
"ValidationRuleSet" Dataset under the Item Revision, and from the Named 
Reference import the example VRX file "validation_rule_example.vrx" that 
is located in NX11 in the following path:


 C:\Program Files\Siemens\NX 11.0\DESIGN_TOOLS\checkmate\tools\ruleset_editor 


Start NX and go through steps to Import an assembly into teamcenter and you 
will then see the "ValidationRuleSet" dataset when you browse.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V11.0
Function: CLONE_IMPORT

Ref: 002-7009329

KB Article ID# PL7009329

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX