Details
---------------
"Save Parts As" dialog in NX integration mode doesn't follow customer default
setting for Save as Action as New Item or New Revision.
Solution
There is a specification change in NX11, now the Table editor dialog in NX11
onwards can be stored in the dialog memory, hence the save as dialog remembers
the last selected options in it.
Note: The Reset button on the Save as dialog can be used to go back to the
customer defaults settings.
Notes and References
IR 8884959
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0.1
Function: FILE_SAVE_AS
Ref: 002-7009326