Unable to create a new Solid Edge file in the SEEC environment

2021-10-06T23:55:27Z

Summary


Details

When attempting to create a new Solid Edge file to be uploaded to Teamcenter, the user is being returned the following error message: “"Teamcenter returned 000000008004A061 which SEEC does not recognize as a known error. Review the log file for further information"”, and the Solid Edge template files are not being 
downloaded to the Solid Edge client.



Solution

This problem can occur if there are multiple folders named “Solid Edge Templates” in Teamcenter. In most cases the folders have been Cut (using Microsoft Ctrl-X, for example) in Teamcenter.  Even though the folders are not seen in the Teamcenter interface, they still exist in the volume.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP9
Function: SEEC

Ref: 002-7009285

KB Article ID# PL7009285

Contents

SummaryDetails

Associated Components