Re-order holes in Synchronous environment

2021-10-06T23:55:12Z

Summary


Details

When modelling Solid Edge Synchronous holes, these holes are put into feature 
groups. Each time the hole feature is used, a new feature group is created 
regardless of the fact that the hole dimension and plane is the same. Each 
group is handled as a pattern when using the part in an assembly. 


There is a need to re-order the holes into one group, so that all these holes 
can be used as a pattern in an assembly.



Solution

 The following workaround will result in a single group for all holes:


1. Select all (identical) holes you want to put into one feature 
2. RMB -> "Break". This will turn all holes into a new face set. 
3. "Recognize Holes". All holes will be listed as one feature (and can be 
modified if needed) 
4. "OK"



Notes and References

ER#1900568



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: SYNC_FEATURES

Ref: 002-7009277

KB Article ID# PL7009277

Contents

SummaryDetails

Associated Components