Graphics display quality is poor when model is rotated

2021-10-06T23:26:55Z

Summary


Details

When the model is rotated, the display quality is poor such that the model 
surfaces appear to have a tearing/twisting appearance to them.



Solution

After verifying the operating system and graphics card were certified, a 
graphics card setting was disabled which resolved the issue.


1. On the desktop background, 'MouseButton3-->NVIDIA Control Panel'. 

2. On the left of the control panel dialog, expand '3D Settings'. 

3. Select 'Manage 3D Settings'. 

4. On the 'Global Settings' tab, scroll down to 'Vertical sync'. 

5. Set 'Vertical Sync' to 'Off'. 

6. Select 'Apply' on the NVIDIA Control Panel dialog.


Disabling this setting allows the monitor and graphics adapter to run at 
their maximum refresh frequencies without having one limit the other. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0
Function: GRAPHICS

Ref: 002-7009248

KB Article ID# PL7009248

Contents

SummaryDetails

Associated Components