NX /allow_null_value is needed in NX 10.0 and up

2021-10-06T23:27:14Z
NX for Design

Summary


Details

--------------- 
Blank values are not overwritten in NX and NX retains last saved values for the 
mapped attributes.



Solution

 In the attribute mapping /allow_null_value is needed in NX 10.0 and up as we 
tightened up this rule and since the old attribute was saved in the part file 
as last time the part was saved in NX, we could not overrate it without 
/allow_null_value.



Notes and References

IR 8801299



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: ATTRIBUTES

Ref: 002-7009143

KB Article ID# PL7009143

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX