How do you view Solid Edge Assembly members in Teamcenter structure manager?

2021-10-06T23:55:29Z

Summary


Details

How do you view Solid Edge Assembly members in the Teamcenter structure manager?



Solution

Make sure to switch on Solid Edge-->Application Button -->Settings-->Manage --> Alternate Assembly Synchronization-->check on Synchronize Alternate position assemblies.


In SEEC create assembly-->Save it. 
Insert child parts. 
Alternate Assemblies--> Create Alternate Positions of the assembly-->Define members using variables.


Save and check-in assembly.


Open this assembly in TC-->Structure manager-->Click on Show/Hide data panel to view assembly.


On the same ribbon bar, there is option view or change the current arrangement for the root assembly click on this Set Current Arrangement window appears to select the required member to visualize.



Notes and References

IR 8006535



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V219.0
Function: COMPONENTS

Ref: 002-7009111

KB Article ID# PL7009111

Contents

SummaryDetails

Associated Components