When opening an Assembly a warning pop-up returns that some Interpart Expressions fail to update.
Solution
This was new to NX10. This is a warning to the user that some Interpart
Expressions have failed to update, and that they will be retained as constants when the assembly is opened.
This can be caused by opening the assembly with Interpart Update toggled OFF, having suppressed components when opening, or components not found using the current load options.
This warning can be disabled by setting the environment variable
UGII_KF_DISABLE_MISSING_IPE_PART_WARNINGS=1
before launching NX.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: PART_FILE_OPS
Ref: 002-7009086