---------------
When you try to open an Insight managed file with Solid Edge you do not see a
folder and so I cannot navigate through the folder structure to open a file.
Why is this the case?
Solution
This is a problem of SharePoint permissions.
Check for your permission (e.g. "Read") in the definition of the
"Permission Level". "View Items" must be checked. By default this is the
case.
In some cases you will need to turn on "Browse Directories" in addition
which is unchecked by default for the "Read" permission .
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 2012_R2
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109.0
Function: INSIGHT
Ref: 002-7009085