Solid Edge Mirrored Assembly Features show incorrect Geometry

2021-10-06T23:55:24Z
ASSEMBLY

Summary


Details

Mirroring a lot of assembly features with a single mirror command showed some 
features - such as holes - which were not mirrored correctly. So not all parts 
showed the same holes, etc.



Solution

If features are dependent on other assembly features, such as holes located on 
"cut" faces, mirroring all of them at the same time can cause problems.


The Workaround is to split the mirror operation into two or more. First mirror 
the "cut" features, afterwards mirror the dependent holes.



Notes and References

PR#7999192



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: ASSEMBLY
Function: FEATURES

Ref: 002-7009082

KB Article ID# PL7009082

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS