The user has found when Populating all members of Family of Parts for a
Sheetmetal part that it generates empty parts. No error is message shown but
the 'Link' symbol is missing in the Family of Parts table.
Solution
Check whether the Sheetmetal option 'Use Gagetable.xls' was enabled and if so
whether the material of the part is not included in 'Gagetable.xls'.
Depending on whether you want to use the gagetable or not:
Either
Disable "Use Gagetable.xls"
Or
Include the material of the part in "Gagetable.xls"
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: FAMILY_OF_PARTS
Ref: 002-7009081